Industrial Software Platform
Infineum

Infineum

The Wonderware IntelaTrac solution at Infineum has allowed the operational procedures for visual inspections of equipment to be optimized and standardized, enabling the plant to achieve a plant availability factor of over 90%.

  • Mauro Tassistro, Applications Team Leader

    Using IntelaTrac has made a major contribution to reaching a plant availability factor above 90%, since it has integrated perfectly with the other innovations added to our equipment.

  • Goals

    • Increase plant’s availability by anticipating any potentially damaging situations
    • Optimize operators’ efficiency and reliability during inspection activity
    • Limit production downtimes to scheduled maintenance only
  • Challenges

    • The proximity of the plants to inhabited areas makes it essential for the sites to be safe and reliable at all times
    • Detection of critical indicators, e.g. vibrations or the presence of foreign particles, which automatic instruments do not usually detect effectively
    • Maximize the value of the time and experience of the field operators
  • Results

    • The Wonderware solution has enabled the plant to achieve a plant availability factor of over 90%
    • The system has allowed the operational procedures for visual inspections of equipment to be optimized and standardized, thanks to the removal of paper reports and the intuitive nature of the handheld devices
    • Wonderware IntelaTrac’s features now allow operators to identify potential problems which were previously neglected, thus avoiding the need for any emergency intervention