Schneider Electric’s industrial software business and AVEVA have combined to create a new global leader in engineering and industrial software. For more details click here.
Industrial Software Platform

Xcellerex

FlexFactory, from Massachusetts based Xcellerex, utilizes Wonderware software to create biotherapeutics and vaccines manufacturing solutions more efficiently.

  • John A. Chickosky, Chief Commercial Officer and President, Biosystems

    With the integration of Wonderware’s software, Xcellerex has been able to deploy FlexFactory® manufacturing capacity, very quickly, resulting in an overall reduction in development time of nearly 60%. This directly impacts customers with reduced costs and shorter time to market. In fact, we’ve been able to reduce deployment time from 3-5 years to an amazing 12-18 months. This results in huge implementation savings and the ability to begin producing high value product 2 to 4 years sooner than traditional technology.

  • Goals

    • Address the growing demands in the biomedical market space for more effective biopharmaceutical manufacturing processes
    • Develop a solution that would define a model for improving how biopharmaceuticals, vaccines and other therapeutics are developed, manufactured and commercialized
  • Challenges

    • Integrating complex technology with ultra-high levels of functionality was considered the greatest challenge in creating a bio manufacturing platform that employs a single-use technology, controlled environment modules, process automation and electronic batch records
  • Results

    • Xcellerex’s FlexFactory enables companies to achieve significant cost savings in several areas, including a capital investment reduction that can exceed 60 percent
    • The solution decreases the facility space required by 40 percent, lessens water usage and waste by 85 percent, and lowers the overall cost of finished products by 32 percent
    • FlexFactory reduces deployment time from three to five years to 12 to 18 months, which enables the production of high value products two to four years sooner than traditional technology
    • The solution achieves an overall reduction in development time of nearly 60 percent, with an estimated 80 percent saving in rework time, which reduces costs and shortens time to market