Norfolk Southern Railway

Norfolk Southern Railway

The Wonderware solution at Norfolk Southern Railway has reduced the development time for the HMI by 40 to 50 percent. It has also increased the work efficiency of both the yardmasters and the trainmasters at the Buckeye trainyard.

  • Tim Forman, Trainmaster Norfolk, Southern Railway

    The new Wonderware system has definitely decreased the labor costs involved with the repair and upkeep of the system on a day-today basis. We’ve been able to remove a lot of old and antiquated equipment we no longer need due to the upgrades in the current software.

  • Goals

    • Operate more than 21,500 route miles in 22 states and Ontario, Canada
    • Completely automate the operation of the trainyard
    • Decrease labor cost and replaces old and antiquated equipmen
  • Challenges

    • Receive up to 2,000 train cars in any given day while assuring efficiency and safety
    • Provide critical information using devices that are easily accessible by trainyard personnel 
  • Results

    • Using the InTouch package, the development time for the HMI was reduced to 40 to 50 percent
    • The new software has increased the work efficiency of both the yardmasters and the trainmasters at Buckeye trainyard