Industrial Software Platform
Società Risorse Idriche Calabresi

Società Risorse Idriche Calabresi

Società Risorse Idriche Calabresi is responsible for a far-reaching system that covers approx. 6,000 kilometers and is comprised of 200 aqueduct systems, 4 dams, 10 derivation crossbars, 14 wastewater plants, 300 lifting stations and almost 1,000 tanks.

  • Sergia De Marco, General Director, Società Risorse Idriche Calabresi

    By the end of the test phase, the Wonderware solution will provide immediate ROI and justify our investment.

  • Goals

    • Increase the capabilities and efficiency of the main plant which supervises a complex regional aqueduct system
    • Better measure water output and gather realtime data to more accurately identify waste
    • Find a flexible and scalable platform to support the entire system
  • Challenges

    • The enormity of the system and the geography of the area makes it difficult to accurately record the volume of water produced
  • Results

    • Società Risorse Idriche Calabresi (So. Ri.Cal. S.p.A.) now monitors and controls a huge system with 200 aqueduct systems, four dams, 10 derivation crossbars, 14 wastewater plants, 300 lifting stations and almost 1,000 tanks
    • The new Wonderware solution brings realtime data to operators in the central plant, allowing them to visualize problems on remote machinery and respond to them immediately and automatically
    • Accurate data is being collected for reporting and analysis, which is valuable for current and future planning
    • With the great success of the pilot program, the Wonderware solution will be implemented across the entire system; immediate ROI is expected