Energy Performance for Manufacturing
As energy expenditures are one of the highest operating expenses in most manufacturing plants, reducing energy consumption can help companies not only reduce operational costs and sustain their competitiveness but also reduce their carbon footprint. Therefore, adopting an effective energy management system is imperative for improved profitability and sustainability.
Based on Schneider Electric’s world-class energy management solution, Energy Performance provides comprehensive visualization tools to reduce energy consumption, optimize equipment utilization and improve electrical network reliability. The platform enables energy data to be merged and synchronized with production events, turning raw data into actionable contextualized insights and uncovering energy efficiency improvement opportunities. In addition, the improved visibility into the equipment electrical performance and power network quality enable the maintenance teams to proactively identify root causes before a failure occurs, reducing unplanned downtime and protecting the plant assets from potential damage.
Energy Performance empowers users to manage energy comsumption with greater precision and accuracy, reducing operational costs and improving profits.