Advanced Process Control for
Mining Minerals & Metals

In today’s economic environment, capital budgets and overhead are constantly being reduced. Companies are faced with rising operating costs, global competition, and soaring energy costs. Advanced Process Control for Mining, Minerals & Metals (APC for MMM) from Schneider Electric is engineered to improve yield, quality, production rates, process stability and reduce specific energy consumption to boost your bottom line.

APC for MMM Addresses these Challenges

APC for MMM enables the operation to function much closer to the operating limits by reducing variations in the process and then maximize value through optimization. The solution simultaneously target the top four major mineral processing concerns:

  • Energy efficiency
  • Recovery and grades or extraction ratio
  • Throughput rates
  • Process stability and Operation standardization

Achieve Peak Operating Performance

Mining companies can now achieve peak efficiency in the operations and processes with APC for MMM by optimizing the high value assets:

  • Maximize production rate and value
  • Improve yield or recovery per unit of feed
  • Minimize specific energy consumption per unit of product
  • Maintain sustainable and safe operation

You Might Also Like

Mining, Minerals and Metals Industry Solutions - Schneider Electric Software

Mining, Minerals and Metals

Schneider Electric delivers solutions that help mining operators meet the volatile and changing market conditions. Schneider Electric’s comprehensive portfolio of solutions, together with our consulting and project management capabilities, help mining operators realize their full potential to create the mine of the future.

Enterprise Supply Chain Software

Unified Supply Chain Management

SimSci Spiral Suite is a modern enterprise supply chain management solution for the Mining, Minerals and Metals (MMM) industries. Developed from the ground up, Spiral Suite is the first solution in the market to provide planning optimization through detailed scheduling in a single unified package, reaching across the pit-to-port supply chain. With a unified approach to planning and scheduling, the solution maximizes the value of collaboration, and establishes a well-governed management process across the enterprise.

Improve-Mining-Operations

Industry Solution: Improve Mining Operations

One opportunity to drive positive change in mining operations has been created through the exponential growth of industrial data and analytics. Organizations can leverage this data to improve performance and efficiency through investments in condition monitoring and predictive analytics solutions. These solutions provide real-time information on the health and performance of critical assets, giving personnel the insight needed to make timely and informed operational and maintenance decisions.

 Performance Excellence for MMM

Industry Solution: Performance Excellence for MMM

Increasing costs, competition and the need to optimize production units are some of the key challenges faced by the Metals, Mining and Minerals industry today.

Grinding circuit

Industry Solution: APC for Grinding Circuit

The Grinding Circuit is one of the most energy intensive areas of mineral processing plants. Learn how APC improve the energy efficiency of the plant.

Floating-Circuit

Industry Solution: APC for Flotation Circuit

A flotation circuit recovers as much of the valuable minerals, and help improve the concentrate quality to the desire grade. Learn how APC improve recovery subject to grade quality constraints.

Thickener

Industry Solution: APC for Thickener

The dewatering processes is to recover process water, which is then treated and recirculated back into the processing plant, and consequently a product with a targeted density or percentage of solids is obtained. Learn how AP improve water recovery.