Schneider Electric’s industrial software business and AVEVA have combined to create a new global leader in engineering and industrial software. For more details click here.
Industrial Software Platform
Enterprise Pipeline Management Solutions
End-To-End Pipeline Management Solutions For Your Oil & Gas Operation

Enterprise Pipeline Management Solutions

Pipelines strive to operate with the highest level of safety (personnel, environment and assets) and reliability (uptime), while increasing operational and cost efficiency and continuing to meet regulatory compliance. Schneider Electric's solutions start with scalable, secure supervisory control at the foundation. We enable operators by providing the most trusted tools to manage day-to-day operation and optimization of hydrocarbon transportation through the supply chain. We offer an integrated, open, end-to-end solution for pipeline management and operations, from the field device-level to operations and into the enterprise, all from a single vendor. 

Our solutions are the most trusted in the industry, managing 60%+ of total hydrocarbon movement in North and Latin America. Our control and monitoring system applications are designed to manage day-to-day activities of crude, refined products, gas and petrochemical pipelines, ensuring safe and efficient operations.

  • Gas Day Operations

    Gas Day Operations

    This offering brings together functionality focused on making sure that the pipeline operations and controllers have the information for gas planning, monitoring and gas control – ensuring supply and demand are balanced and capacity is optimized.

  • Gas Measurement and Analysis System - Measurement Advisor

    Gas Measurement and Analysis System - Measurement Advisor

    Measurement Advisor brings together a suite of applications focused on making sure that the pipeline controller, measurement and gas operations has the required information to manage their pipeline assets in a safe, reliable and most efficient way.

  • Integrity Operations

    Integrity Operations

    Integrity Operations is built on the SimSuite framework, which brings together a suite of applications focused on making sure that the Pipeline Controller has the required leak prevention, detection and mitigation tools when operating the pipeline.

  • OASyS DNA - SCADA (Pipeline Edition)

    OASyS DNA - SCADA (Pipeline Edition)

    This overarching application supports the Enterprise Pipeline Management Solutions (EPLMS) framework. It seamlessly integrates operations under a single umbrella of centralized, standardized hardware and software. Users experience a uniform, intuitive interface offering vital information in real time.

  • Pipeline Operations (Liquids Edition)

    Pipeline Operations (Liquids Edition)

    Pipeline Operations (Liquids Edition) brings together a suite of applications focused on making sure that the pipeline controller has the required operational tools to allow them the operate the pipeline asset in real time from the control room.

  • Pipeline Operations (Gas Edition)

    Pipeline Operations (Gas Edition)

    Pipeline Operations (Gas Edition) brings together operational business logic to the control room for natural gas gathering, transmission and distribution networks.

  • Pipeline Trainer

    Pipeline Trainer

    Pipeline Trainer brings together a suite of applications focused on making sure that the pipeline controller has the required qualifications to manage the expensive pipeline assets they have been designated to operate.