Schneider Electric’s industrial software business and AVEVA have combined to create a new global leader in engineering and industrial software. For more details click here.
Industrial Software Platform

Gas Measurement and Analysis System - Measurement Advisor

Gas Measurement and Analysis System - Measurement Advisor is a gas flow measurement software that enables gas pipeline operations to accurately and efficiently collect & validate measurement data – enabling billing your customers via automated data acquisition of gas history and gas quality, validation, re-calculations, audit trails and pre-financial verification and correction of disparate field data. It improves flow measurement accuracy and reliability by identifying and reducing metering errors and facilitates reporting for both measurement analyst & department as well as for internal and regulatory purposes. Measurement Advisor also identifies and helps reduce lost and unaccounted for (LAUF) gas.

A single, centralized device configuration of measurement gas control, Measurement Advisor is an integrated solution from a single vendor which brings together gas day forecasting, flow measurement, polling and SCADA. An integrated validation engine ensures gas flow measurement and gas control data is trusted (ensuring Measurement Data Validation Integrity).

Key capabilities of Gas Measurement and Analysis System - Measurement Advisor:

  • Improves Measurement Data Integrity - flexibility to recalculate, extrapolate and estimate missing measurement data - (ie: faulty flow computer or meter) to ensure data integrity and accuracy is as high as possible
  • Enables measurement validation in real time - apply programmed validation rules to immediately detect erroneous measurement data, resulting in addressing critical issues as measurement data is collected from the field – reducing time to correction and potential measurement losses
  • Helps identify and minimize the Gas Lost and unaccounted for  (LAUF)
  • Utilizes segment and system-wide balancing to allow measurement analysts to quickly identify mass, volume and energy in/out errors
  • Simplifies end-of-month reporting by producing volumetric accounting reports for the full accounting closing process after validation of the final data each month
  • Facilitates Regulatory Compliance and Audits

You Might Also Like

OASyS DNA

Schneider Electric OASyS DNA

This overarching application supports the Enterprise Pipeline Management Solutions (EPLMS) framework. It seamlessly integrates operations under a single umbrella of centralized, standardized hardware and software. Users experience a uniform, intuitive interface offering vital information in real time.

Pipeline Integrity

Schneider Electric Integrity Operation

Schneider Electric Integrity Operation is built on the SimSuite framework, a part of our Enterprise Pipeline Management Solutions (EPLMS) which brings together a suite of applications focused on making sure that the Pipeline Controller has the required leak prevention, detection and mitigation tools when operating the pipeline.

Pipeline Operation - Liquids

Schneider Electric Pipeline Operation – Liquids

As a part of our Enterprise Pipeline Management Solutions (EPLMS), Pipeline Operation Liquids brings together a suite of applications focused on making sure that the pipeline controller has the required operational tools to allow them the operate the pipeline asset in real time from the control room.

Natural Gas and Gas Day Operation

Schneider Electric Pipeline Operation – Natural Gas

As a part of our Enterprise Pipeline Management Solutions (EPLMS), Pipeline Operation – Natural Gas brings together operational business logic to the control room for natural gas gathering, transmission and distribution networks.

Pipeline Trainer

Schneider Electric Pipeline Trainer

As a part of our Enterprise Pipeline Management Solutions (EPLMS), Pipeline Trainer brings together a suite of applications focused on making sure that the pipeline controller has the required qualifications to manage the expensive pipeline assets they have been designated to operate.

Gas Day Operations

Schneider Electric Gas Day Operations

This offering, which is a part of our Enterprise Pipeline Management Solutions (EPLMS), brings together functionality focused on making sure that the pipeline operations and controllers have the information for gas planning, monitoring and gas control – ensuring supply and demand are balanced and capacity is optimized.