Industrial Software Platform

Pipeline Operations (Gas Edition)

Pipeline Operations (Gas Edition), a gas pipeline management software, adds gas industry operational business logic to the control room for natural gas gathering, transmission and distribution networks. From up-to-the-minute flow rate calculations and flow totals, to real-time calculation and monitoring of line pack, storage, and compressor performance, these applications provide current information to SCADA controllers in a highly available redundant environment, integrated with the power of OASyS DNA.

Key capabilities of Pipeline Operations:

  • Data acquisition adapted for Gas Industry including Gas History, Gas Quality and related Industry Standard and specific protocols.
  • Real-time metering/analysis supporting configuration of ‘Host Calculated” flow meters and gas chromatographs allowing the system to calculate corrected flow rates in volume and energy units, heating values and specific gravity on a real-time basis.
  • Real-time flow totals monitoring station total flow rates, plant or other facility fuel usage, gas processing plant shrinkage, line segment inventory changes, and other operational functions.
  • Line pack monitoring allowing a segment-by-segment scan of operating pressures and temperatures along the pipeline to calculate the current line pack and pack/draft values in real time.

You Might Also Like

OASyS DNA

Schneider Electric OASyS DNA

This overarching application supports the Enterprise Pipeline Management Solutions (EPLMS) framework. It seamlessly integrates operations under a single umbrella of centralized, standardized hardware and software. Users experience a uniform, intuitive interface offering vital information in real time.

Pipeline Integrity

Schneider Electric Integrity Operation

Schneider Electric Integrity Operation is built on the SimSuite framework, a part of our Enterprise Pipeline Management Solutions (EPLMS) which brings together a suite of applications focused on making sure that the Pipeline Controller has the required leak prevention, detection and mitigation tools when operating the pipeline.

Pipeline Operation - Liquids

Schneider Electric Pipeline Operation – Liquids

As a part of our Enterprise Pipeline Management Solutions (EPLMS), Pipeline Operation Liquids brings together a suite of applications focused on making sure that the pipeline controller has the required operational tools to allow them the operate the pipeline asset in real time from the control room.

Gas Measurement and Analysis System

Schneider Electric Gas Measurement and Analysis System (GMAS)

As a part of our Enterprise Pipeline Management Solutions (EPLMS), GMAS brings together a suite of applications focused on making sure that the pipeline controller, measurement and gas operations has the required information to manage their pipeline assets in a safe, reliable and most efficient way.

Pipeline Trainer

Schneider Electric Pipeline Trainer

Schneider Electric Pipeline Trainer, a part of our Enterprise Pipeline Management Solutions (EPLMS), brings together a suite of applications focused on making sure that the pipeline controller has the required qualifications to manage the expensive pipeline assets they have been designated to operate.

Gas Day Operations

Schneider Electric Gas Day Operations

This offering, which is a part of our Enterprise Pipeline Management Solutions (EPLMS), brings together functionality focused on making sure that the pipeline operations and controllers have the information for gas planning, monitoring and gas control – ensuring supply and demand are balanced and capacity is optimized.