Industrial Software Platform

Schneider Electric Pipeline Trainer

The more complex a pipeline becomes, the more challenging it is to manage problems that drain the bottom line and expose companies to painful publicity and regulatory scrutiny. Leading pipeline operators know the best defense is a good offense: establish the best possible predictive, preventive, and protective measures — and then make sure to have highly trained pipeline controllers in place to implement those measures.

Operator Training Simulators (OTS) based on advanced modeling and simulation tools are essential in both developing a control room management (CRM) plan and in training pipeline controllers. Many leading pipeline operators have found the answer to their training needs in Schneider Electric Pipeline Trainer, built on the SimSuite framework, ensuring knowledge capture and transfer and at the same time improving safety and reducing risk.

Schneider Electric Pipeline Trainer, a part of our Enterprise Pipeline Management Solutions (EPLMS), brings together a suite of applications focused on making sure that the pipeline controller has the required qualifications to manage the expensive pipeline assets they have been designated to operate.

Key capabilities of Pipeline Trainer:

  • Ability to model accurately the control logic and malfunctions associated with field devices & SCADA sequencing – giving a more realistic control room response
  • Can be used on any type of pipeline due to 2-phase simulation engine (Built on SimSuite framework)
  • Ability to provide Generic, Hybrid and Full Scope Trainer

You Might Also Like

OASyS DNA

Schneider Electric OASyS DNA

This overarching application supports the Enterprise Pipeline Management Solutions (EPLMS) framework. It seamlessly integrates operations under a single umbrella of centralized, standardized hardware and software. Users experience a uniform, intuitive interface offering vital information in real time.

Pipeline Integrity

Schneider Electric Integrity Operation

Schneider Electric Integrity Operation is built on the SimSuite framework, a part of our Enterprise Pipeline Management Solutions (EPLMS) which brings together a suite of applications focused on making sure that the Pipeline Controller has the required leak prevention, detection and mitigation tools when operating the pipeline.

Pipeline Operation - Liquids

Schneider Electric Pipeline Operation – Liquids

As a part of our Enterprise Pipeline Management Solutions (EPLMS), Pipeline Operation Liquids brings together a suite of applications focused on making sure that the pipeline controller has the required operational tools to allow them the operate the pipeline asset in real time from the control room.

Natural Gas and Gas Day Operation

Schneider Electric Pipeline Operation – Natural Gas

As a part of our Enterprise Pipeline Management Solutions (EPLMS), Pipeline Operation – Natural Gas brings together operational business logic to the control room for natural gas gathering, transmission and distribution networks.

Gas Measurement and Analysis System

Schneider Electric Gas Measurement and Analysis System

The Gas Measurement and Analysis Solutions (GMAS) is a gas flow measurement software that enables gas pipeline operations to accurately and efficiently collect & validate measurement data – enabling billing your customers.

Gas Day Operations

Schneider Electric Gas Day Operations

This offering, which is a part of our Enterprise Pipeline Management Solutions (EPLMS), brings together functionality focused on making sure that the pipeline operations and controllers have the information for gas planning, monitoring and gas control – ensuring supply and demand are balanced and capacity is optimized.