Schneider Electric’s industrial software business and AVEVA have combined to create a new global leader in engineering and industrial software. For more details click here.
Industrial Software Platform

SimSci PIPEPHASE

PIPEPHASE is a steady-state, multiphase fluid flow simulation solution for rigorous modeling of gathering networks and pipeline systems. This solution can model applications ranging from single well sensitivity analyses of key parameters to a multi-year planning study for an entire production field. PIPEPHASE improves profitability and performance in companies across the globe by using proven solution algorithms, modern production methods and software analysis techniques to create a robust and efficient oil field design and planning tool.

You Might Also Like

SimSci DYNSIM

SimSci DYNSIM

DYNSIM is dynamic process simulation software enabling process design, operational analysis, control check and Operator Training Simulation (OTS).

SimSci SIM4ME Portal

SimSci SIM4ME Portal

The SIM4ME Portal integrates SimSci software with Microsoft Excel, extending the Return on Investment (ROI) with additional functionality.

SimSci Dynamic Simulation Suite

SimSci Dynamic Simulation Suite

SimSci Dynamic Simulation Suite (DSS) provides dynamic simulation and control system emulation and consists of DYNSIM, TRISIM Plus, SCP270 and Logic Validator.

SimSci DYNSIM Power

SimSci DYNSIM Power

DYNSIM Power is an advanced, unified power plant modeling simulation used throughout the life of a power plant by creating dynamic simulation models.