SimSci SimCentral
SimCentral is the innovative, integrated simulation platform covering the entire plant engineering lifecycle of design, simulation & training, and optimization. The current release of SimCentral focuses on utilities modeling for steam systems, cooling water systems, and flare networks. Users can now streamline process utility design and better collaborate for process improvement. They can also ease modeling complexity to cut costs, while delivering a user experience that empowers and appeals to the engineers now entering the workforce. SimCentral provides models that can be simulated and improved upon faster, with greater accuracy while avoiding future capital expenditures.
- SimCentral models can be solved in either steady state or dynamic simulation.
- SimCentral allows custom modeling to simulate new equipment and plant types, or new phenomena, such as water hammer.
SimCentral for Process Utilities is the first release in decades that comprises a process simulator built from the ground up. It offers an intuitive user experience far superior than competitive offerings to uniquely address the needs of Engineering, Procurement and Construction (EPC) firms, Operating companies and Process Licensors. It is the first commercially available platform designed to take advantage of developing web-based and cloud technologies while delivering a modern user experience. SimCentral for Process Utilities embraces the expectations of the next generation of users to accelerate adoption, usage and time-to-value.