Schneider Electric’s industrial software business and AVEVA have combined to create a new global leader in engineering and industrial software. For more details click here.
Industrial Software Platform

SimSci Upstream Optimization Suite (UOS)

The Upstream Optimization Suite (UOS) of products provide tools to support field-wide production analysis from sandface-to-surface facilities. Utilizing PIPEPHASE and NETOPT, UOS' integrated approach allows time-sensitive process conditions and events to be factored into on-line optimization models. Integrated data reconciliation fosters statistical detection and elimination of gross data errors or ‘drift’. The suite supports unidirectional data sharing and exchange with many legacy systems and incorporates a COM-compliant Applications Programming Interface (API) for integration with third-party tools.

You Might Also Like

SimSci PIPEPHASE

SimSci PIPEPHASE

PIPEPHASE provides a steady-state, multiphase fluid flow simulation solution for rigorous modeling of gathering networks and pipeline systems.

SimSci DYNSIM

SimSci DYNSIM

DYNSIM is dynamic process simulation software enabling process design, operational analysis, control check and Operator Training Simulation (OTS).

SimSci SIM4ME Portal

SimSci SIM4ME Portal

The SIM4ME Portal integrates SimSci software with Microsoft Excel, extending the Return on Investment (ROI) with additional functionality.

SimSci DYNSIM Power

SimSci DYNSIM Power

DYNSIM Power is an advanced, unified power plant modeling simulation used throughout the life of a power plant by creating dynamic simulation models.