SimSci Dynamic Simulation Suite (DSS)

Dynamic Simulation Suite (DSS) provides rigorous dynamic simulation and control system emulation for engineering studies. The applications comprising DSS enables validation of control system design before it is installed in the plant, eliminating many problems that occur during startup and shutdown. The DSS solution supports skill development and improved plant design and performance.

You Might Also Like

SimSci DYNSIM

SimSci DYNSIM

DYNSIM is dynamic process simulation software enabling process design, operational analysis, control check and Operator Training Simulation (OTS).

SimSci TRISIM Plus

SimSci TRISIM Plus

SimSci TRISIM Plus is a “Virtual Simulation” of Triconex Trident and Tricon controllers and TRI-GP that provides a reduced time to commission and improved startup.

SimSci SCP270

SimSci SCP

SimSci SCP is for the “Virtual Simulation” of Foxboro Control Processors CP270 and CP280 for designing and troubleshooting.

SimSci Logic Validator

SimSci Logic Validator

SimSci Logic Validator is an automated test harness aimed at automating safety logic validation of Safety Instrumented Systems (SIS) per the International Society of Automation standard ISA-S84.