Schneider Electric’s industrial software business and AVEVA have combined to create a new global leader in engineering and industrial software. For more details click here.
Industrial Software Platform

SimSci Logic Validator

The Logic Validator is an automated test harness aimed at automating safety logic validation of safety Safety Instrumented Systems (SIS) per the International Society of Automation standard ISA-S84. The Logic Validator automatically executes a series of commands that sets tag or input variables, allows a loop to process and verifies the outcome matches expectations. It is designed to work in a soft or simulated environment separate from the real DCS or PLC hardware.

You Might Also Like

Unified Power Plant Modeling Simulation from SimSci DYNSIM Power - Schneider Electric Software

SimSci DYNSIM Power

DYNSIM Power is an advanced, unified power plant modeling simulation used throughout the life of a power plant by creating dynamic simulation models.

SimSci DYNSIM Dynamic Process Simulator - Schneider Electric Software

SimSci DYNSIM

DYNSIM is dynamic process simulation software enabling process design, operational analysis, control check and Operator Training Simulation (OTS).

Virtual Simulation of Triconex Trident and Tricon controllers from SimSci TRISIM Plus - Schneider Electric Software

SimSci TRISIM Plus

SimSci TRISIM Plus is a “Virtual Simulation” of Triconex Trident and Tricon controllers and TRI-GP that provides a reduced time to commission and improved startup.

Virtual Simulation of I/A Series DCS Control Processor from SimSci SCP270 - Schneider Electric Software

SimSci SCP

SimSci SCP is for the “Virtual Simulation” of Foxboro Control Processors CP270 and CP280 for designing and troubleshooting.

OperatorTraining Simulators from SimSci - Schneider Electric Software

SimSci Operator Training Simulators

Operator Training Simulators (OTS) are advanced computer-based training tools that help give operators the skills they need to run a process or plant.