Schneider Electric’s industrial software business and AVEVA have combined to create a new global leader in engineering and industrial software. For more details click here.
Industrial Software Platform

SimSci TRISIM Plus

TRISIM Plus is a “Virtual Simulation” of Triconex Trident and Tricon controllers and TRI-GP combined with the base modeling capability from DYNSIM. This simulator allows access to emulation available in the TriStation 1131 version 4 series software. This software provides a redinvuced time to commission and improved startup. TRISIM Plus is delivered with Schneider Electric's turnkey Operator Training Simulator (OTS) or for use by Triconex Trident and Tricon users for safety and turbomachinery (TMC) control checkout.

You Might Also Like

SimSci Dynamic Simulation Suite - Schneider Electric Software

SimSci Dynamic Simulation Suite

SimSci Dynamic Simulation Suite (DSS) provides dynamic simulation and control system emulation and consists of DYNSIM, TRISIM Plus, SCP and Logic Validator.

SimSci DYNSIM Dynamic Process Simulator - Schneider Electric Software

SimSci DYNSIM

DYNSIM is dynamic process simulation software enabling process design, operational analysis, control check and Operator Training Simulation (OTS).

Virtual Simulation of I/A Series DCS Control Processor from SimSci SCP270 - Schneider Electric Software

SimSci SCP

SimSci SCP is for the “Virtual Simulation” of Foxboro Control Processors CP270 and CP280 for designing and troubleshooting.

Logic Validator

SimSci Logic Validator

SimSci Logic Validator is an automated test harness aimed at automating safety logic validation of Safety Instrumented Systems (SIS) per the International Society of Automation standard ISA-S84.

Control System Design Chekout from SimSci DYNSIM Checkout | Schneider Electric Software

SimSci DYNSIM Checkout

DYNSIM Checkout supports validation of control system design before it is installed in the plant to eliminate many of the problems that occur during startup.