SimSci Optimize
ROMeo, part of the Online Performance Suite (OPS), is the real-time optimization tool from SimSci.

Process Optimization

SimSci Optimization solutions monitor performance, control and obtain peak performance to deliver the maximum benefit in large and complex process plants where the scale and complexity requires formal solutions.

  • Advanced Process Control (APC) software uses both realtime and historical data to analyze, identify, and model the significant cause-and-effect relationships in a process. SimSci APC uses this information to reduce variations in the process, allowing for operation much closer to the operation limits which improves process profitability.
  • Process Optimization software uses real-time process and economic data to determine set points that guarantee maximum operating profit while satisfying all regulatory requirements. ROMeo employs first principle simulation techniques with proven data reconciliation and optimization technologies to provide maximum, sustainable plant performance and increased return on investment.

Engineers can use a validated model to continually evaluate and improve processes with respect to their efficiency, effectiveness and flexibility, thus reducing overall risk and boosting profitability. Access to key performance data, in a timely manner, improves performance and competitiveness through better operational decision-making and new insights into optimization potentials.

  • SimSci Online

    SimSci Online

    SimSci Online is a cloud based solution which provides the same high-quality simulation software as the on-premise solution.

  • SimSci APC

    SimSci APC

    SimSci APC reduces variations in the process, allowing for operation much closer to the operation limits which improves process profitability and control.

  • SimSci ROMeo Online Performance Suite

    SimSci ROMeo Online Performance Suite

    Performance enhancing solutions based on ROMeo’s real-time optimization capabilities that allow customers to remain competitive.

  • SimSci Integration with Off-sites

    SimSci Integration with Off-sites

    Integration between Off-sites and ROMeo allows actual crude blend assay and other properties to be passed directly into ROMeo online optimization software.

  • SimSci Spiral CrudeSuite Integration with ROMeo

    SimSci Spiral CrudeSuite Integration with ROMeo

    Optimize feedstock selection using accurate models to judge the impact of various feedstock.

  • SimSci LPVector

    SimSci LPVector

    The LP Yield Vector capability of ROMeo provides a feature for passing base and delta yield vector data from ROMeo to linear planning models commonly used in refining.

  • SimSci Off-sites

    SimSci Off-sites

    SimSci refinery Off-sites solutions provide accurate, reliable and accessible inventory and movement information, movement automation and off-line/on-line multi-blend optimization.

  • SimSci Performance Analysis, Diagnostics and Optimization

    SimSci Performance Analysis, Diagnostics and Optimization

    Performance Analysis, Diagnostics and Optimization (PADO) presents real-time and historical performance information to the entire power generating enterprise in a concise and timely manner.

  • SimSci ROMeo Gas Plant Process Manager

    SimSci ROMeo Gas Plant Process Manager

    ROMeo Gas Plant Process Manager (GPPM) uses a model-based approach to manage productivity geared towards optimizing gas plant performance.

  • SimSci ROMeo Crude Unit Performance Monitoring Bundle

    SimSci ROMeo Crude Unit Performance Monitoring Bundle

    ROMeo Crude Unit Process Manager (CUPM) uses a model-based approach to optimize crude unit performance and productivity.

  • SimSci ROMeo Material Balance Module

    SimSci ROMeo Material Balance Module

    The ROMeo Material Balance Module (MBM) provides mass and volume reconciliation, converting real-time process data into reliable information.

  • SimSci ROMeo Process Optimization

    SimSci ROMeo Process Optimization

    ROMeo Process Optimization provides real-time optimization for the refining, petrochemical and gas processing industries.

  • SimSci ROMeo Reactor Models

    SimSci ROMeo Reactor Models

    ROMeo Reactor Models is a plant-wide optimization solution, delivering increased refining profits by optimizing refining process units.

  • SimSci ROMeo Utilities Optimization

    SimSci ROMeo Utilities Optimization

    The ROMeo Utilities Optimization solution is used to optimize performance in plants by minimizing usage of steam, water, fuel and other utilities.

  • SimSci SIM4ME Portal

    SimSci SIM4ME Portal

    The SIM4ME Portal integrates SimSci software with Microsoft Excel, extending the ROI with additional functionality.

  • SimSci Yield Accounting

    SimSci Yield Accounting

    Schneider Electric Yield Accounting Solution increases accuracy and reliability for receipt, shipment and process data and identifies gross errors, corrects inaccuracies and reduces losses.