Industrial Software Platform

Production and Accumulator Optimization Module

The automatic Production and Accumulator Optimization module minimizes operational cost of the district heating network by constantly choosing the best production scenario to ensure minimum production cost.

The module continuously performs a load prediction (for example based on weather forecast information downloaded from the Internet), taking into account  the heat volume supplied to the consumers in the network while also using the flexibility and dynamics provided by the accumulator tank.

It also provides for the accumulated heat loss and energy consumption in the network and the hydraulic constraints as defined in Termis.

Operational Cost Savings

  • Reduces energy costs by approximately 5-10% depending on the flexibility and variation in fuels
  • Improves your economy and reduces CO2 emission
  • Reduces maintenance work required, leading to an extension of the life span of these units

The module requires limited or no intervention. The module is in operation around the clock. Save money all the time – every single day of the year.

You Might Also Like

Chilled Water Network Real-Time Simulator

Termis Chilled Water Network Real-Time Simulator

The Termis Chilled Water Network Real-Time Simulator software calculates energy loss and operational cost, validates measurement points and can be used to make decisions for future operations of the Chilled Water plants.

Temperature Optimization Module

Termis Temperature Optimization Module

The Termis Temperature Optimization Module minimizes heat loss and operational costs in the district heating network. The inlet temperature is adjusted to be as low as possible, taking into account the amount of heat that has to be supplied to the consumers in the net.

Customer Case Study Veolia China

Termis Customer Case Study - Veolia China Depends on Termis for Overview of District Heating Network

“We use Termis to provide an overview of the whole district heating network hydraulic characteristics.” Read the full case study here.

Customer Fact Utility

Termis Customer Fact - Utility Uses Termis for Energy Savings Reporting

Olgod Tekniske Vaerker selected Termis because it provides the capability to report energy savings points. Read the full customer fact here.